Data Block ConstTeSysIsland
The data block ConstTeSysIsland serves as a global storage of constants relevant across multiple function blocks. Currently it only contains the definition of the common set of status and error codes that are used by all function blocks. See Function Blocks for a description of each of the function blocks contained in this library and details about which error and status codes are used by the function block.
To avoid unintended behavior of the function blocks, this data block is protected against changes to the values contained within it. To review the contents of the data block, double-click on it. If prompted for a password, choose Cancel. As protected function blocks within a library are pre-compiled for a type of Siemens® PLC, the function block library contains one Master copy for each PLC type that the library is designed for. All Master copies of the DataBlock (DB) contain the same members and values.
Content of Data Block ConstTeSysIsland
|
Member |
Data Type |
Value |
Description |
|
Cdw_ErrNoMsg |
DWORD |
16#0000 |
Error code: No error message available |
|
Cdw_ErrInternal |
DWORD |
16#1101 |
Error code: Internal function block error detected |
|
Cdw_ErrInvalidCycInAddr |
DWORD |
16#1201 |
Error code: Invalid start address for cyclic input data configured |
|
Cdw_ErrInvalidHwid |
DWORD |
16#1202 |
Error code: Invalid HWID for acyclic communication configured (Details in q_dwAcyclicStatus) |
|
Cdw_ErrInvalidNumOfAvatars |
DWORD |
16#1203 |
Error code: Invalid number of avatars specified (i_uiNoConfAvatar must be less or equal 20) |
|
Cdw_ErrReadCycIn |
DWORD |
16#1301 |
Error code: Error reading cyclic input data |
|
Cdw_ErrReadAcycData1 |
DWORD |
16#1401 |
Error code: Error reading acyclic data set 1 (Details in q_dwAcyclicStatus) |
|
Cdw_ErrReadAcycData2 |
DWORD |
16#1402 |
Error code: Error reading acyclic data set 2 (Details in q_dwAcyclicStatus) |
|
Cdw_ErrWriteAcycData |
DWORD |
16#1481 |
Error code: Error writing acyclic data set (Details in q_dwAcyclicStatus) |
|
Cdw_StsNoMsg |
DWORD |
16#0000 |
Status code: No status details available |
|
Cdw_StsReadAcycData1Compl |
DWORD |
16#2001 |
Status code: Reading acyclic data set 1 completed successfully |
|
Cdw_StsReadAcycData2Compl |
DWORD |
16#2002 |
Status code: Reading acyclic data set 2 completed successfully |
|
Cdw_StsWriteAcycDataCompl |
DWORD |
16#2081 |
Status code: Writing acyclic data set completed successfully |