DOCA0272EN-00

Document Scope

This user guides provides:

  • instructions for configuring a TeSys™ island device within the Siemens® Totally Integrated Automation (TIA) Portal environment.

  • characteristics of the Siemens SIMATIC S7–1200 CPUs and PROFINET IO as bus systems. The basic principles remain the same when using PROFIBUS DP or S7–1500 PLCs as they are for the bus systems above. The process for handling other systems can vary. This guide outlines these differences.

  • information of TeSys island IEC 61131-3 function block libraries for Siemens TIA Portal. These libraries mainly consist of function blocks that can be used to control, monitor, and diagnose the avatars and devices of a TeSys island from within a PLC program written in Siemens TIA Portal.

  • details on the interfaces of said function blocks as well as an introduction to their usage to aid in creating such a PLC program. It also defines the requirements and prerequisites that need to be met to use the function blocks.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?