PN_Starter_AssetMgmt (PROFINET IO)
Inputs
|
Input |
Data Type |
Description |
Variable Category |
|---|---|---|---|
|
i_xEnable |
BOOL |
Activates the function block processing. Cyclic data will be read/written to the hardware IO interface. |
Function block control |
|
i_xAcyclicBusy |
BOOL |
Can be used to block the acyclic execution if acyclic communication of another function block is active. |
Function block control |
|
i_xExecute |
BOOL |
Starts an acyclic request on a rising edge. |
Function block control |
|
i_hwSubmHWID |
HW_IO |
Must correspond to the hardware identifier of the of the related device to be able to execute the acyclic communication. |
Communication parameter |
Outputs
|
Output |
Data Type |
Description |
Variable Category |
|---|---|---|---|
|
q_xActive |
BOOL |
If this output is set to TRUE, the Avatar function block is enabled, or an acyclic request is busy. |
Function block status |
|
q_xError |
BOOL |
If this output is set to TRUE, a detected error occurred while executing the Avatar function block. For detailed information about the detected error, see the value of the Error ID. |
Function block status |
|
q_dwErrorID |
DWORD |
The Error ID shows detailed information about the detected error that occurred. Possible values are shown in the table below. |
Function block status |
|
q_dwAcyclicStatus |
DWORD |
The Acyclic status provides detailed information about the acyclic fieldbus communication, including detected error details. For detailed information about the status values, see Function Block Library. |
Function block status |
|
q_xAcyclicBusy |
BOOL |
If this output is set to TRUE, an acyclic request is still busy. |
Function block status |
|
q_udtProductData |
UDT_ProductData |
Contains all relevant product data of the device. |
Acyclic data |
|
q_udiTimeOn |
UDINT |
The length of time that the device has been switched on. |
Acyclic data |
|
q_udiTimeSwitchOn |
UDINT |
The length of time that the contactor has been switched on. |
Acyclic data |
|
q_uiNumDevEvt |
UINT |
The number of detected device events. |
Acyclic data |
|
q_udiNumContClose |
UDINT |
The number closing cycles of the contactor. |
Acyclic data |
|
q_udiNumDevicePowOn |
UDINT |
The number of device power cycles. |
Acyclic data |
|
q_uiMaxIrms |
UINT |
The maximum measured current value during device lifetime. |
Acyclic data |
|
q_udiAvgIrms |
UDINT |
The calculated average current value. |
Acyclic data |