DOCA0356EN-00

About the Document

Document Scope

This document provides complete information necessary to install, commission, and maintain the TeSys Tera system which includes:

  • LTMT main unit

  • LTMTCT/LTMTCTV sensor module
  • LTMT expansion unit
  • LTMTCUF control operator unit.

The purpose of this guide is to:

  • Familiarize yourself with the mechanical characteristics of the components of TeSys Tera system.

  • Describe how to assemble and wire the TeSys Tera system and its components.

  • Describe how to commission and maintain the TeSys Tera system.

This guide is intended for:

  • Design engineers

  • Panel builders

  • System integrators

  • Maintenance engineers

NOTE: The product image captured in this guide is for Ethernet variant of the TeSys Tera system, which will be available in the future releases. Please contact your local Schneider Electric representative concerning its availability.

Validity Note

This document is valid for the following certified components of the TeSys Tera system

  • LTMTMFM: LTMT main unit with Modbus RTU protocol, 100–240 Vac/Vdc

  • LTMTMBD: LTMT main unit with Modbus RTU protocol, 24 Vdc

  • LTMTPFM: LTMT main unit with PROFIBUS DP protocol, 100–240 Vac/Vdc

  • LTMTPBD: LTMT main unit with PROFIBUS DP protocol, 24 Vdc

    @Updated D3
  • LTMTCT3T: LTMT Sensor Module with current transformer, current range = 0.3–3 A.

  • LTMTCT25T: LTMT Sensor Module with current transformer, current range = 2.5–25 A.

    @Updated D3
  • LTMTCT100T: LTMT Sensor Module with current transformer, current range = 10–100 A.

    @Updated D3
  • LTMTCTV3T: LTMT Sensor Module with current and voltage transformers, current range = 0.3–3 A, voltage range = 60–690 Vac

  • LTMTCTV25T: LTMT Sensor Module with current and voltage transformers, current range = 2.5–25 A, voltage range = 60–690 Vac

  • LTMTCTV100T: LTMT Sensor Module with current and voltage transformers, current range = 10–100 A, voltage range = 60–690 Vac

  • LTMTCTV3UT: LTMT Sensor Module with current and voltage transformers, current range = 0.3–3 A, voltage range = 60–600 Vac

  • LTMTCTV25UT: LTMT Sensor Module with current and voltage transformers, current range = 2.5–25 A, voltage range = 60–600 Vac

  • LTMTCTV100UT: LTMT Sensor Module with current and voltage transformers, current range = 10–100 A, voltage range = 60–600 Vac

  • LTMTIN42FM: LTMT expansion unit with four digital inputs and two digital outputs, 100–240 Vac/Vdc

  • LTMTIN42BD: LTMT expansion unit with four digital inputs and two digital outputs, 24 Vdc

  • LTMT9RJ1015: LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable 0.15 m (5.9 in.) in length

    @Updated D3

  • LTMT9RJ401: LTMT main unit to LTMT expansion unit RJ45 connector cable 0.1 m (3.9 in.) in length

    @Updated D3

  • LTMT9RJ105: LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable 0.5 m (19.6 in.) in length

    @Updated D3

  • LTMTCUF: LTMTCUF control operator unit

  • LTMT9RJ102: LTMT main unit to LTMTCT/LTMTCTV sensor module cable 0.2 m (78.74 in.) in length

  • LTMT9EX10: LTMT main unit to LTMT expansion unit cable 1 m (39.37 in.) in length

  • LTMT9CU10S: LTMT main unit to LTMTCUF control operator unit 1 m (39.37 in.) in length

    @Updated D3
  • LTMT9CU30S: LTMT main unit to LTMTCUF control operator unit 3 m (118.11 in.) in length.

    @Updated D3

The certification of other components of the TeSys Tera system mentioned in this document is in progress.

The availability of some functions described in this document depends on the communication protocol used and the physical modules installed on the TeSys Tera system.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Environmental Data

For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.

Available Languages of the Document

The document is available in these languages:

  • English

Related Documents

Title of documentation

Description

Reference number

TeSys Tera Motor Management System Catalog

The catalog

  • Describes the TeSys Tera system

  • Contains the TeSys Tera technical characteristics

LVCATENTER

TeSys Tera Motor Management System User Guide

This is the main user guide that introduces the complete TeSys Tera system. It describes the main functions of the LTMT main units, LTMTCT/LTMTCTV sensor modules, LTMT expansion units, and LTMTCUF control operator unit.

DOCA0257EN

TeSys Tera Motor Management System Modbus RTU Communication Guide

This guide describes the Modbus network protocol communication of the LTMT main unit.

DOCA0355EN

TeSys Tera Motor Management System PROFIBUS DP Communication Guide

This guide describes the PROFIBUS DP network protocol communication of the LTMT main unit.

DOCA0256EN

TeSys Tera Motor Management System LTMTCUF control operator unit User Guide

This guide describes how to install, configure, and use the LTMTCUF control operator unit.

DOCA0233EN

TeSys Tera Motor Management System DTM library Online Help Guide

This guide describes the TeSys Tera DTM Library which allows the customization of the control functions of the TeSys Tera Motor Management System.

DOCA0275EN

TeSys Tera Motor Management System DTM library Software Release Notes

This document provides important information about the TeSys Tera DTM Library software and provides summary of new features and enhancement.

DOCA0279EN

TeSys Tera Motor Management System Firmware Release Notes

This guide provides important information about the TeSys Tera system firmware packages and provides summary of new features and enhancement.

DOCA0276EN

To find documents online, visit the Schneider Electric download center www.se.com/ww/en/download/.

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademarks

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?