First Setup Parameters
The TeSys Tera system required parameters can be configured by using:
-
A PC running the TeSys Tera DTM embedded in a FDT container such as SoMove software: go to Parameter List > General Settings to configure the required parameters.
For more information, refer to the TeSys Tera Motor Management System DTM Library Online Help Guide – DOCA0275EN.
-
The LTMTCUF control operator unit: go to Menu > First Setup to configure the required parameters.
For more information, refer to the TeSys Tera Motor Management System LTMTCUF Control Operator Unit User Guide – DOCA0233EN:
Configure the required parameters in the following order:
-
Device configuration.
-
Starter settings.
-
System settings.
-
Communication settings.
-
Date time settings.
-
-
The device configuration, starter settings, and system settings are described in the user guide. For more information, refer to the TeSys Tera Motor Management System User Guide – DOCA0257EN.
-
The communication settings are described in user guide. For more information, refer to the TeSys Tera Motor Management System User Guide – DOCA0257EN.
Device Configuration
The device configuration consists of selecting:
-
Reference of the LTMTCT/LTMTCTV sensor module connected to the LTMT main unit
-
Temperature type configuration of LTMT main unit
The device configuration are described in the user guide. For more information, refer to the TeSys Tera Motor Management System User Guide – DOCA0257EN.
After configuring the references of the modules connected to the LTMT main unit, the device LED on the LTMT main unit must be green.
If the device LED on the LTMT main unit is not green, use the TeSys Tera DTM and go to Diagnostics > Diagnostic Data > Device Internal Status to correct the error detected.
If the device LED on the LTMT main unit is green and no errors are detected, the other required parameters can be configured.
Starter Settings
The starter type configured by default is the Direct Online starter. If another starter type is required, then select the required starter type from the list of starter types.
To set the other starter settings, refer to the TeSys Tera Motor Management System User Guide – DOCA0257EN.
System Settings
The system settings configure:
-
System characteristics (nominal voltage, nominal frequency, and nominal power).
-
Motor characteristics (full load current, phase rotation).
-
External CT characteristics.
To set the system settings, refer to the TeSys Tera Motor Management System User Guide – DOCA0257EN.
Communication Settings
The communication settings of the device can be configured via:
-
A PC running the TeSys Tera DTM embedded in a FDT container such as SoMove software.
-
The LTMTCUF control operator unit.
-
A PLC or DCS via the communication.