DOCA0356EN-00

Connection of the LTMT Main Unit to PC

Use USB/RJ45 cable to connect USB port of the PC running the TeSys Tera DTM to the RJ45 port marked HMI on the LTMT main unit.

NOTE: Please contact your local Schneider Electric representative concerning the availability of the EtherNet/IP variant.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?