DOCA0356EN-00

Connection of LTMT Main Unit to LTMTCUF Control Operator Unit

To provide connections for both the communication signals and the power supply:

  1. Mount the LTMTCUF control operator unit

  2. Connect it to LTMT main unit via the RJ45 port at the rear of the unit to the RJ45 port marked HMI on the LTMT main unit.

It is possible to connect a PC to the LTMTCUF control operator unit via the RJ45 port on the front face of the unit.

The following section describes how to connect the LTMTCUF control operator unit to both the LTMT main unit and a PC.

Connecting to the LTMT Main Unit

Use the cable LTMT9CU10S or LTMT9CU30 to connect the LTMTCUF control operator unit to the RJ45 port marked HMI of the LTMT main unit front face.

@ Updated image D3

NOTE: Please contact your local Schneider Electric representative concerning the availability of the EtherNet/IP variant.

A

Backside of LTMTCUF control operator unit

B

Grounding collar

C

LTMT9CU10S or LTMT9CU30 HMI device connection cable

D

LTMT main unit

Connecting to a PC

Connect a PC to the LTMTCUF control operator unit via the RJ45 on the front face of the unit.

@ Updated image D3

NOTE: Please contact your local Schneider Electric representative concerning the availability of the EtherNet/IP variant.

A

PC running the TeSys Tera DTM embedded in a FDT container, such as SoMove software

B

USB/RJ45 cable

C

LTMTCUF control operator unit

D

Grounding collar

E

LTMT9CU10S or LTMT9CU30 HMI device connection cable

F

LTMT main unit

NOTE:

When the LTMTCUF control operator unit is connected to a PC, the LTMTCUF control operator unit becomes passive and cannot be used to display information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?