DOCA0356EN-00

Additional Parameters

Introduction

In addition to the first setup parameters, configure the below parameters if required at first power-up or later:

  • Protection settings.

  • I/O Settings.

For more information, refer to the TeSys Tera Motor Management System User Guide – DOCA0257EN.

LTMTCUF Control Operator Unit

In the LTMTCUF control operator unit, first setup and other parameters are located in the sub-menus of the Menu.

TeSys Tera DTM

In the TeSys Tera DTM, first setup and other parameters are located in tree view items in the My Device > Parameters List tab.

@updated d3
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?