DOCA0356EN-00

Connection Guidelines

The following wiring guidelines must be respected to reduce disturbance on the behavior of the TeSys Tera system due to EMC:

  • Keep sufficient distance as possible between the communication cable and the power and/or control cables (minimum 30 cm or 11.8 in.).

  • Cross over different types of cables at right angles, if necessary.

  • Do not bend or damage the cables. The maximum bending radius is 10 times the cable diameter.

  • Avoid sharp angles of paths or passages of the cable.

  • To reduce EMI effect connect the communication cable shield to a protective ground at both ends.

  • Keep the connection of the cable shield as short as possible.

  • Several shields can be connected together.

  • Perform the grounding of the shield with a collar.

  • Place the cable along the grounded plate around the withdrawable drawer.

Connection Cables

NOTICE
UNINTENDED EQUIPMENT OPERATION
Use Schneider Electric standard cables.
Failure to follow these instructions can result in equipment damage.

The following table lists the connection cables of TeSys Tera system:

@Updated D3

Reference number

Cable description

Cable type

Cable length

LTMT9RJ1015

LTMT main unit to LTMTCT/LTMTCTV sensor module

RJ11

0.2 m (7.8 in.)

LTMT9RJ105

LTMT main unit to LTMTCT/LTMTCTV sensor module

RJ11

0.5 m (19.6 in.)

LTMT9RJ401

LTMT main unit to LTMT expansion units

RJ45

0.1 m (3.9 in.)

LTMT9RJ102
LTMT main unit to LTMTCT/LTMTCTV sensor module RJ45 0.2 m (78.74 in)

LTMT9EX10

LTMT main unit to LTMT expansion unit RJ45 1 m (39.37 in.)

LTMT9CU10S

LTMT main unit to LTMTCUF control operator unit

RJ45 1 m (39.37 in.)

LTMT9CU30S

LTMT main unit toLTMTCUF control operator unit HMI RJ45 3 m (118.11 in.)

PC to LTMT main unit

USB/RJ45

2.5 m (98.42 in.)

TSXPBSCA•00

PROFIBUS DP connecting cable

Shielded twisted pair

100 m (3937 in.)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?