DOCA0356EN-00

Communication Alarms and Trips

Introduction

Communication alarms and trips are managed in a standard way, like any other types of alarms and trips.

The presence of a trip is signaled by various indicators:

  • State of the communication LED on LTMT main unit

  • Alarm

  • Message(s) displayed on LTMTCUF control operator unit

Network Communication Loss

A communication loss is managed like any other trip. For more information, refer to TeSys Tera Motor Management System User Guide – DOCA0257EN.

HMI Communication Loss

HMI Communication loss Function:

  • Detects the loss of communication between the LTMT main unit and the HMI connected via the HMI port, once communication has been established.

  • Generates an alarm or a trip action according to the function setting.

Parameter Setting

Parameter Range Default Value
Function
  • Disable

  • Alarm

  • Trip

  • Alarm and Trip

Disable
Time delay 0.1 – 6000.0 s in ste of 0.1s 1 s
Reset mode
  • Auto

  • Reset Key

  • DI

  • Communication

Reset Key + DI
@Updated D3
Auto Rest delay 0.0 – 6000.0 s in step of 0.1 s 0.0 s
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?