Unboxing Guidelines
Opening the Box
The box contains the TeSys Tera modules and respective accessories which are shown in the below image.
-
Modules: LTMT main unit, LTMT expansion unit, LTMTCUF control operator unit, and cables.
-
Light Instruction Sheet
Modules and Cables |
In the Box |
LTMT main unit |
|
LTMTCT/LTMTCTV sensor module The box also contains two screws for mounting the LTMT main unit on top of the sensor module. |
|
LTMT expansion unit |
|
LTMTCUF control operator unit |
|
LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable |
|
LTMT main unit to LTMT expansion unit RJ45 connector cable |
|
LTMT main unit to LTMTCUF control operator unit connection cable |
Peelable Label Instructions
The peelable label is on the front face of the LTMT main unit.
-
Read the following instructions printed on the label before removing it:
WARNING
UNINTENDED EQUIPMENT OPERATION- Ensure the DO contacts of the LTMT main unit are set to the Normally Open (NO) position using a multi meter.
- Ensure to provide auxiliary power supply to the LTMT main unit before applying the motor control voltage.
Failure to follow these instructions can result in death, serious injury, or equipment damage.Terminal Details Expected State Verify between O3 NO and O3 C2 NO Verify between O3 NC and O3 C2 NC Verify between O1 13 and C1 14 NO Verify between O2 23 and C1 14 NO -
To remove the peelable label, hold the notch provided and peel the label off the LTMT main unit
NOTE: Please contact your local Schneider Electric representative concerning the availability of the EtherNet/IP variant.