DOCA0356EN-00

Wiring Guidelines

The following wiring guidelines must be respected to reduce disturbance due to EMC on the behavior of the LTMT main unit:

  • Keep sufficient distance as possible between the communication cable and the power and/or control cables (minimum 30 cm or 11.8 in.).

  • Cross over different types of cables at right angles, if necessary.

  • Do not bend or damage the cables. The maximum bending radius is 10 times the cable diameter.

  • Avoid sharp angles of paths or passage of the cable.

  • Use shielded cables to connect ground fault current transformers:

    • The cable shield must be connected to a protective ground at both ends.

    • The connection of the cable shield to the protective ground must be as short as possible.

    • Connect together all the shields, if necessary.

    • Perform the grounding of the shield with a collar.

  • Systematically add filters on contactor coils.

For more information, refer to chapter ElectroMagnetic Compatibility (EMC) in Electrical Installation guide (available in English only) and Okken and Blockset guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?