Compatibility Check of Device/Firmware and Corrective Actions
ToDo @Gregory: Check if EPC content needs to be updated
Overview
When ULP modules are upgraded with new functionalities, verify with the EcoStruxure Power Commission software that they are compatible with the different modules in the IMU system. Use the table to perform diagnostics and identify discrepancies between the ULP modules. This table also provides the recommended actions relevant to the detected discrepancies.
To view the firmware status, click in the Device view.
|
Legend |
Name |
Description |
|---|---|---|
|
A |
|
Displays the IP address of the connected device. |
|
B |
|
Displays the Modbus address of the connected device. |
|
C |
|
Lists the ULP modules of the connected device. |
|
D |
|
Displays the compatibility status of the module inside the system. |
|
E |
|
Displays the current firmware version installed in the module. |
|
F |
|
Displays the latest firmware version available for upgrade. |
|
G |
|
Provides the solution for discrepancies. |
|
H |
Refresh |
Updates the changes made as per the recommended action. |
Status
The column identifies the discrepancy conditions within the ULP modules.
Recommended Actions
The Recommended action to be performed column provides a solution to resolve a discrepancy. Each discrepancy has a generic predefined recommended action.
The table lists the recommended actions to take in the case of a detected discrepancy.
|
Module status |
Description |
Recommended action to be performed |
|---|---|---|
|
Nominal |
The ULP module is in nominal mode. |
None. |
|
Non-critical firmware discrepancy |
There is a non-critical firmware discrepancy between the ULP module and other modules in the IMU. |
Upgrade firmware at the next maintenance operation. |
|
Non-critical hardware discrepancy |
There is a non-critical hardware discrepancy between the ULP module and other modules in the IMU. |
Replace module at the next maintenance operation. |
|
Critical firmware discrepancy |
There is a critical firmware discrepancy between the ULP module and other modules in the IMU. |
Upgrade firmware. |
|
Critical hardware discrepancy |
There is a critical hardware discrepancy between the ULP module and other modules in the IMU. |
Replace module. |
|
Hardware degraded |
The ULP module is in degraded mode. |
Replace module at the next maintenance operation. |
|
Stop |
The ULP module is out of service. |
Replace module. |
|
Conflict |
The ULP module is in conflict mode. |
Remove duplicate module. |
Refresh
After performing a recommended action for a specific discrepancy, you can click the button to update the changes in the window.