Daisy-Chained Distributed Modbus Architecture
The following figure shows an example of a daisy-chained distributed Modbus architecture with seven IMUs:
-
An IMU consisting of a PowerPacT P- and R-frame circuit breaker and an IFM interface.
-
Six IMUs consisting of a PowerPacT H-, J-, and L-frame circuit breaker, an IFM interface, and an FDM121 display each.
|
A |
Modbus cable coming from Modbus client |
|
B |
24 Vdc AD power supply for MicroLogic trip units in MasterPacT NT/NW or PowerPacT P- and R-frame circuit breakers |
|
C |
Shunt terminal block on the incoming supply |
|
D |
24 Vdc ABL8 power supply for ULP modules |
|
E |
Modbus cable running to first cubicle |
|
F |
NSX cord |
|
G |
RJ45 plug ULP cord |
|
H |
RJ45 Modbus T-junction |
|
I |
IFM interface |
|
J |
Modbus cable running to second cubicle |
|
K |
Modbus line termination |
For a distributed Modbus architecture, RJ45 Modbus T-junction can be used to connect the upstream Modbus cable and the downstream Modbus cable.
Shunt Terminal Block on the Incoming Supply
The shunt terminal block on the incoming supply can connect the Modbus cable and the power supply for all the IMUs.
The shunt terminal block consists of four 5-channel spring terminal blocks.
|
A |
24 Vdc power supply |
|
B |
Modbus cable coming from Modbus client |
|
C |
Clip-on plastic end stop |
|
D |
End plate |
|
E |
Spring terminal block |
|
F |
Modbus cable running to first cubicle |
The following table lists the part numbers for the shunt terminal block:
|
Component |
Nominal cross-section |
Part number |
|---|---|---|
|
5-channel spring terminal block |
2.5 mm2 (14 AWG) |
NSYTRR24D+NSYTRALV24 (gray) |
|
End plate |
– |
AB1 RRNACE244 |
|
Clip-on plastic end stop |
– |
AB1 AB8R35 |
Modbus Cable Connection
-
The Modbus cable coming from the Modbus client ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).
-
The Modbus cable running to the first cubicle ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail) for the cubicle.
The 24 Vdc power supply running to the first cubicle ensures continuity of the power supply.
-
The unused channel on the shunt terminal block can be used to connect another Modbus server in the electrical equipment (a PM800 communicating power meter, for example).
Wiring Diagram of Shunt Terminal Block on the Incoming Supply
|
A |
24 Vdc power supply |
|
B |
Modbus cable coming from Modbus client |
|
C |
24 Vdc power supply cable running from Modbus servers |
|
D |
Modbus cable running to Modbus servers |
|
E |
24 Vdc power supply cable running to Modbus servers |
Modbus Cable Lengths for a Single Power Supply Segment
|
A |
Shunt terminal block on the incoming supply |
|
B |
Modbus line termination |
The total length of all L2s must be less than L1.
Case of Several Power Supply Segments
When more than one 24 Vdc power supply is needed (refer to segmented power), then several power supply segments are used along the Modbus cable.
|
A |
Modbus cable coming from Modbus client |
|
B |
24 Vdc AD power supply for MicroLogic trip units in MasterPacT NT/NW or PowerPacT P- and R-frame circuit breakers |
|
C |
Shunt terminal block on the incoming supply |
|
D |
24 Vdc ABL8 power supply for ULP modules |
|
E |
Modbus cable running to first cubicle |
|
F |
NSX cord |
|
G |
RJ45 plug ULP cord |
|
H |
RJ45 Modbus T-junction |
|
I |
IFM interface |
|
J |
Modbus cable running to second cubicle |
|
K |
Modbus cable running to third cubicle |
|
L |
Shunt terminal block on the cubicle incomer |
|
M |
Modbus line termination |
Shunt Terminal Block on the Incomer of the Third Cubicle
The shunt terminal block on the incomer of the third cubicle can be used to connect a new 24 Vdc power supply to power the IMUs in the third cubicle.
The shunt terminal block consists of four 5-channel spring terminal blocks.
|
A |
24 Vdc power supply |
|
B |
Modbus cable coming from second cubicle |
|
C |
Clip-on plastic end stop |
|
D |
End plate |
|
E |
Spring terminal block |
|
F |
Modbus cable rising up the third cubicle |
Modbus Cable Connection
-
The Modbus cable from the Modbus client ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).
-
The Modbus cable running to the first cubicle ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail) for the cubicle.
The 24 Vdc power supply running to the first cubicle ensures continuity of the power supply for the cubicle.
-
The Modbus cable running to the second cubicle ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail) for the second cubicle.
The 24 Vdc power supply running to the second cubicle ensures continuity of the power supply for the second cubicle.
-
The Modbus cable running to the third cubicle ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).
A separate 24 Vdc power supply is connected to the third cubicle.
Wiring Diagram of Shunt Terminal Block on the Incomer of the Third Cubicle
|
A |
24 Vdc power supply |
|
B |
Modbus cable coming from second cubicle |
|
C |
Modbus cable rising up the third cubicle |
|
D |
24 Vdc power supply cable rising up the third cubicle |
Modbus Cable Lengths for Several Power Supply Segments
|
A |
Shunt terminal block on the cubicle incomer |
|
B |
Modbus line termination |
Modbus cable L3 ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).
The total length of all L2s must be less than L1 in the corresponding installation.