0602IB1503-03

IFM Interface with Part Number STRV00210

Introduction

The IFM interface with part number STRV00210 is substituted by the IFM interface with part number LV434000.

The following table shows the specificities for each IFM interface.

Characteristics

IFM interface STRV00210

IFM interface LV434000

Circuit breaker compatibility

  • MasterPacT NT/NW

  • PowerPacT P- and R-frame

  • PowerPacT H-, J-, and L-frame

  • MasterPacT NT/NW

  • PowerPacT P- and R-frame

  • PowerPacT H-, J-, and L-frame

  • MasterPacT MTZ

Modbus connector

5-pin

RJ45

Cable

Free-ends Modbus cable

RJ45 Modbus cables

Modbus circuit

D0, D1, common C, power supply

D0, D1, 0 VL common

Connection of the 0 V common to a ground terminal block

Yes, ground terminal block required.

No, given that 0 VL is isolated.

Modbus isolation

Two-wire RS 485 isolated repeater required

No repeater required

Modbus line termination

Screwed

RJ45

The specific features of IFM interface with part number STRV00210 , including rules for ULP connection and power supply, are detailed in this appendix.

Hardware Description

A

5-pin screw type connector (Modbus connection and power supply)

B

Modbus address rotary switches

C

Modbus traffic LED

D

Modbus locking pad

E

ULP LED

F

Test button

G

Mechanical lock

H

Two RJ45 ULP ports

I

Stacking accessory

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?