ULP Modules
ULP Modules
ULP modules can be grouped in categories:
-
Generic ULP modules which are compliant with all circuit breakers as presented in the following tables.
-
ULP modules specific to PowerPacT H-, J-, and L-frame circuit breakers.
-
ULP modules specific to MasterPacT NT/NW and PowerPacT P- and R-frame circuit breakers.
IFE Ethernet Interface for One Circuit Breaker
The IFE Ethernet interface for one circuit breaker provides an Ethernet access to a single intelligent modular unit using a PowerPacT or MasterPacT circuit breaker.
Each circuit breaker has its own IFE interface and a corresponding IP address.
|
Illustration |
Part number |
Documentation |
|---|---|---|
|
LV434001 |
|
IFE Ethernet Switchboard Server
The IFE Ethernet switchboard server provides an Ethernet access to one or several intelligent modular units using PowerPacT or MasterPacT circuit breakers.
It supports the following communication architectures:
-
One single circuit breaker connected to the IFE server.
-
Up to 11 circuit breakers through IFM Modbus-SL interfaces that are stacked to the IFE server.
|
Illustration |
Part number |
Documentation |
|---|---|---|
|
LV434002 |
|
IFM Modbus-SL Interface for One Circuit Breaker
The IFM Modbus-SL interface provides access to a Modbus serial line communication network for a single intelligent modular unit using a PowerPacT or MasterPacT circuit breaker.
|
Illustration |
Part number |
Documentation |
|---|---|---|
|
LV434000 |
Instruction sheet: NVE85393 |
IO Input/Output Application Module for One Circuit Breaker
The IO input/output application module for one circuit breaker is one of the components of the ULP architecture.
The IO application module enhances control and monitoring functions of a single intelligent modular unit with a PowerPacT or MasterPacT circuit breaker due to its built-in applications. Its resources are:
-
Six digital inputs: self-powered inputs, used as NO and NC dry contact or pulse counter.
-
Three digital outputs: bistable relay (5 A maximum).
-
One analog input for Pt100 temperature sensor.
|
Illustration |
Part number |
Documentation |
|---|---|---|
|
LV434063 |
|
FDM121 Front Display Module for One Circuit Breaker
The FDM121 front display module for one circuit breaker shows the measurements, alarms, and operating assistance data from a single intelligent modular unit with a PowerPacT or MasterPacT circuit breaker.
|
Illustration |
Part number |
Documentation |
|---|---|---|
|
STRV00121 |
|
UTA Tester
The UTA tester is used to set up, test, and maintain a single intelligent modular unit with a PowerPacT H-, J-, and L-frame circuit breaker and the associated ULP modules.
|
Illustration |
Part number |
Documentation |
|---|---|---|
|
STRV00911 |
Instruction sheet: 48940-330-01 |
Service Interface
The Service Interface is a portable instrument designed for field testing.
The Service Interface is used for:
-
Configuration of Enerlin'X devices
-
Testing and configuration of MicroLogic trip units mounted in the following low voltage circuit breakers:
-
MasterPacT NT/NW circuit breakers
-
EasyPact MVS circuit breakers
-
ComPacT NS circuit breakers
-
PowerPacT P- and R- frame circuit breakers
-
ComPacT NSX circuit breakers
-
PowerPacT H-, J-, and L- frame circuit breakers
-
|
Illustration |
Part number |
Documentation |
|---|---|---|
|
LV485500 |
|
RJ45 ULP Ports
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
ULP modules have RJ45 ports, identified by one of the following pictograms:
Updating the Firmware in ULP Modules
The user can update the firmware of a ULP module by using the latest version of EcoStruxure Power Commission software.
The compatibility matrix embedded in EcoStruxure Power Commission software helps the user to perform diagnostics and correct the firmware discrepancy issues between the ULP modules by providing recommended actions and diagnostics messages relevant to the detected discrepancies.
-
The firmware of the BSCM circuit breaker status control module.
-
The firmware of the MicroLogic trip units installed in MasterPacT NT/NW and PowerPacT P- and R-frame circuit breakers.