0602IB1503-03

ULP System Presentation

Description

Use the ULP (Universal Logic Plug) system to construct an electrical distribution solution which integrates metering, communication, and operating assistance functions for circuit breakers.

Legend

Description

Part of the ULP system

A

FDM128 Ethernet display for eight devices

B

FDM121 front display module for one circuit breaker

C

IFE Ethernet interface for one circuit breaker

D

IFE Ethernet switchboard server

E

IFM Modbus-SL interface for one circuit breaker

F

IO input/output application module for one circuit breaker

G

MasterPacT MTZ drawout circuit breaker

H

MasterPacT MTZ fixed circuit breaker

I

MasterPacT NT/NW circuit breaker

J

PowerPacT P- and R-frame circuit breaker

K

PowerPacT H-, J-, and L-frame circuit breaker

L

ULP port module for MasterPacT MTZ circuit breakers

M

EIFE embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker

N

ULP line termination

O

RJ45 plug/plug ULP cord

P

Circuit breaker BCM ULP cord

Q

NSX cord

R

Ethernet switch

S

Panel server

T

BCM ULP circuit breaker communication module

U

Cord between ULP port module and EIFE interface

V

MicroLogic control unit for MasterPacT MTZ circuit breakers

W

MicroLogic trip unit for MasterPacT NT/NW and PowerPacT P- and R-frame circuit breakers

X

MicroLogic 5 or 6 trip unit for PowerPacT H-, J-, and L-frame circuit breakers

Y

PC with EPC software for test and commissioning of the IMUs

Cable

Description

Ethernet network

Modbus network

ULP network

24 Vdc power supply

Features

Use the ULP system to enhance the functions of PowerPacT H-, J-, and L-frame, PowerPacT P- and R-frame, MasterPacT NT/NW, and MasterPacT MTZ circuit breakers by:

  • An Ethernet communication link for access and remote monitoring with the IFE interface or EIFE interface (MasterPacT MTZ drawout circuit breakers only).

  • Web access to monitor and control the circuit breaker connected to an IFE interface or EIFE interface (MasterPacT MTZ circuit breakers only).

  • An input/output application with an IO module. It benefits from the extended capability of the IO module to monitor and control position of drawout circuit breakers in the cradle, circuit breaker operation, and custom application, and so on.

  • Test, setup, and maintenance functions with EcoStruxure Power Commission software.

  • A Modbus-SL communication link for access and remote monitoring with the IFM interface.

  • Local display of measurements and operating assistance data with the FDM121.

The ULP system lets the circuit breakers become a metering and supervision tool to assist energy efficiency and can:

  • Optimize energy consumption by zone or by application, according to the load peaks or priority zones.

  • Improve electrical equipment management.

Intelligent Modular Unit (IMU)

A modular unit is a mechanical and electrical assembly containing one or more products to perform a function in electrical equipment (incoming protection, motor command, and control). The modular units are easily installed in the electrical equipment.

The circuit breaker with its internal communicating components (for example, MicroLogic trip unit) and external ULP modules (for example, IO module) connected to one communication interface (IFM, IFE, or EIFE depending on the circuit breaker type) is called an IMU.

Examples of IMU with PowerPacT Circuit Breaker

Example 1: IMU composed of a fixed PowerPacT H-, J-, or L-frame circuit breaker connected to an IFM interface and an FDM121 display.

A

IFM Modbus-SL interface for one circuit breaker

B

NSX cord

C

NSX cord terminal block (included with NSX cord)

D

MicroLogic trip unit

E

BSCM circuit breaker status control module

F

RJ45 plug ULP cord

G

ULP line termination

H

FDM121 front display module for one circuit breaker

Example 2: IMU composed of a drawout PowerPacT H-, J-, or L-frame circuit breaker connected to one IO module for cradle management and an IFE interface.

A

IFE Ethernet interface for one circuit breaker

B

ULP line termination

C

RJ45 plug ULP cord

D

NSX cord

E

CE/CD (connected/disconnected) position auxiliary switches

F

Support for two moving connectors

G

9-wire moving connector

H

9-wire fixed connector for base

I

IO input/output application module for one circuit breaker

Examples of IMU with MasterPacT NT/NW Circuit Breaker

Example 1: IMU composed of a fixed, electrically-operated MasterPacT NT circuit breaker connected to an IFM interface and an FDM121 display.

A

IFM Modbus-SL interface for one circuit breaker

B

Circuit breaker BCM ULP cord

C

Fixed terminal block

D

BCM ULP circuit breaker communication module

E

Fixed electrically-operated circuit breaker

F

RJ45 plug ULP cord

G

ULP line termination

H

FDM121 front display module for one circuit breaker

Example 2: IMU composed of a drawout MasterPacT NT circuit breaker connected to one IO module for cradle management and an IFE interface.

A

IFE Ethernet interface for one circuit breaker or IFE Ethernet switchboard serve

B

ULP line termination

C

RJ45 plug ULP cord

D

Circuit breaker BCM ULP cord

E

Circuit breaker disconnected position contact (CD)

F

Circuit breaker cradle

G

BCM ULP circuit breaker communication module

H

Drawout circuit breaker

I

Drawout terminal block

J

Circuit breaker connected position contact (CE)

K

Circuit breaker test position contact (CT)

L

IO input/output application module for one circuit breaker

Examples of IMU with MasterPacT MTZ Circuit Breaker

Example 1: IMU composed of a MasterPacT MTZ fixed circuit breaker connected to one IO module and an IFE interface.

A

IFE Ethernet interface for one circuit breaker or IFE Ethernet switchboard server

B

ULP line termination

C

IO input/output application module for one circuit breaker

D

RJ45 plug ULP cord

E

ULP port module

F

MasterPacT MTZ fixed circuit breaker

Example 2: IMU composed of a MasterPacT MTZ drawout circuit breaker connected to an EIFE interface and one IO module.

A

IO input/output application module for one circuit breaker

B

ULP line termination

C

ULP port module

D

RJ45 plug ULP cord

E

MasterPacT MTZ drawout circuit breaker

F

Cord between ULP port module and EIFE interface

G

EIFE embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?