Presentation of ULP System Architectures
Introduction
The ULP system architecture is defined by the way in which the Ethernet or Modbus-SL network interconnects the intelligent modular units (IMUs).
The various possible ULP system connections define four architectures.
-
Standalone architecture: the IMUs are not communicating to communication interfaces (IFE, EIFE, or IFM interfaces).
-
Centralized Modbus architecture: the IMUs are communicating to communication interfaces (IFE servers and IFM interfaces). The IFE servers and IFM interfaces are grouped in islands, mounted side-by-side on a DIN rail and interconnected by the stacking accessory.
-
Distributed Modbus architecture: the IMUs are communicating to IFM interfaces. The IFM interfaces are distributed as close as possible to the ULP modules in the IMU and linked by the Modbus cable.
There are two possible configurations for the distributed Modbus architecture:
Both these distributed architectures can be combined to form a mixed architecture.
-
Daisy-chained Ethernet architecture: the IMUs are communicating to IFE or EIFE interfaces. The IFE and EIFE interfaces are distributed as close as possible to the ULP modules in the IMU and linked by the Ethernet cable.
-
Star Ethernet architecture: the IMUs are communicating to IFE or EIFE interfaces. The IFE or EIFE interfaces are distributed as close as possible to the ULP modules in the IMU and linked by the Ethernet cable to the switch.
The distributed and centralized architectures can be combined to adapt to the electrical installation and its restrictions.
The ULP system architectures follow rules for building low-voltage switchboards in compliance with ANSI C37.20.1 and UL 1558, UL 845, and UL 891 standards.
Choice of Architecture
The following table lists the advantages and disadvantages of ULP system architectures:
|
Architecture |
Advantages |
Disadvantages |
|---|---|---|
|
Centralized Modbus |
|
Need for a dedicated place in the cubicle where the IFM interfaces can be grouped. |
|
Daisy-chained distributed Modbus |
|
|
|
Tap-linked distributed Modbus |
|
|
|
Daisy-chained Ethernet |
|
|
|
Star Ethernet |
|
|