0602IB1503-03

Centralized Modbus Architecture

Introduction

In a centralized Modbus architecture, the intelligent modular units (IMUs) are communicating to communication interfaces (IFE servers or IFM interfaces). The IFE servers and IFM interfaces are grouped in islands, mounted side-by-side on a DIN rail, and interconnected by the stacking accessory.

Centralized Modbus Architecture

The following figure shows an example of a centralized Modbus architecture with three IMUs:

  • An IMU consisting of a PowerPacT P- and R-frame circuit breaker, and an IFE Ethernet switchboard server to get an Ethernet connection.

  • An IMU consisting of a PowerPacT H-, J-, and L-frame circuit breaker, an IFM interface, and an FDM121 display.

  • An IMU consisting of a PowerPacT H-, J-, and L-frame circuit breaker, an IO module, an IFM interface, and an FDM121 display.

A

24 Vdc AD power supply for MicroLogic trip units in MasterPacT NT/NW or PowerPacT P- and R-frame circuit breakers

B

24 Vdc ABL8 power supply for ULP modules

C

IO module

D

IFM interfaces grouped with stacking accessories

E

Modbus line termination

F

IFE server

G

RJ45 plug ULP cord

Cable

Description

Ethernet network

ULP network

24 Vdc power supply

Modbus Cable Connection

If there is no IFE server in the centralized architecture, connect the Modbus cable as shown in the following figure.

A

Modbus line termination

B

24 Vdc power supply

C

Modbus cable coming from Modbus client

D

ULP line termination

Cable

Description

Modbus network

ULP network

24 Vdc power supply

The Modbus cable coming from the Modbus client is connected to an IFM interface. It ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).

Wiring Diagram

The following wiring diagram shows the connections for the Modbus cable and the 24 Vdc power supply:

A

24 Vdc power supply

B

Modbus line termination

C

IFM interface

D

Modbus cable coming from Modbus client

E

Ground connection at end of Modbus cable when the Modbus client is installed in the same electrical equipment as the IFM interfaces to which it is connected

For information about cable shield management, refer to the rules for Modbus connection linking several pieces of electrical equipment.

IFE Ethernet Switchboard Server Power Supply

When the IFE server is stacked to the IFM interfaces, the 24 Vdc power supply of the IFE server and the serial line Modbus communication are distributed to the IFM interfaces.

Cable

Description

Ethernet network

ULP network

24 Vdc power supply

Wiring Diagram for IFE Ethernet Switchboard Server

The following wiring diagram shows the connections for the IFE server and the 24 Vdc power supply in detail:

A

24 Vdc power supply

B

Modbus line termination

C

IFM interface

D

IFE server

Case of a Single Power Supply Segment

The following figure shows a centralized Modbus architecture with two cubicles and a single power supply segment:

A

24 Vdc ABL8 power supply for ULP modules

B

Modbus cable coming from Modbus client

C

NSX cord

D

IFM interface

E

Modbus cable running to second cubicle

F

Modbus line termination

Cable

Description

Modbus network

ULP network

24 Vdc power supply

Modbus Cable Connection with a Single Power Supply Segment

  • The Modbus cable coming from the Modbus client is connected to an IFM interface. It ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).

  • The Modbus cable running to the second cubicle can be connected to any IFM interface in the group. It ensures continuity of the Modbus signal to the second cubicle and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).

    The 24 Vdc power supply cable running to the second cubicle can be connected to any IFM interface in the group. It ensures continuity of the 24 Vdc power supply to the second cubicle.

Wiring Diagram with a Single Power Supply Segment

The following wiring diagram shows the connections for the Modbus cables and the 24 Vdc power supply in the case of a single power supply segment:

A

24 Vdc power supply

B

Ground connection at end of Modbus cable when the Modbus client is installed in the same electrical equipment as the IFM interfaces to which it is connected

C

Modbus cable coming from Modbus client

D

IFM interface

E

Modbus line termination

For information about cable shield management, refer to the rules for Modbus connection linking several pieces of electrical equipment.

Case of Several Power Supply Segments

When more than one 24 Vdc power supply is needed (refer to segmented power), then several power supply segments are used along the Modbus cable.

The following figure shows a centralized Modbus architecture with three power supply segments:

A

24 Vdc ABL8 power supply for ULP modules

B

Modbus cable coming from Modbus client

C

IFM interfaces grouped with stacking accessories

D

Modbus cable running to second cubicle

E

Modbus cable running to third cubicle

F

Modbus line termination

Cable

Description

Modbus network

ULP network

24 Vdc power supply

Connection of Modbus Cable with Several Power Supply Segments

  • The Modbus cable coming from the Modbus client ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).

  • The Modbus cable running to the second cubicle ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).

    A separate 24 Vdc power supply is connected to the second cubicle.

  • The Modbus cable running to the third cubicle ensures continuity of the Modbus signal (D0, D1, and 0 VL) and shield continuity by using brass clamps. The brass clamps must have suitable diameter for the cable type and fixings compatible with the installation (for example, screw or DIN rail).

    A separate 24 Vdc power supply is connected to the third cubicle.

Wiring Diagram with Several Power Supply Segments

The following wiring diagram shows the connections for the Modbus cables and the 24 Vdc power supply in the case of several power supply segments:

A

24 Vdc power supply

B

Ground connection at end of Modbus cable when the Modbus client is installed in the same section of electrical equipment as the IFM interfaces to which it is connected

C

Modbus cable coming from Modbus client

D

IFM interface

E

Modbus cable between pieces of electrical equipment

F

Modbus line termination

For information about cable shield management, refer to the rules for Modbus connection linking several pieces of electrical equipment.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?