Composition Rules for IMUs
Introduction
Connection of an IMU in the ULP system is simple, but must comply with the rules concerning composition, RJ45 plug/plug ULP cords, and the ULP module power supply.
General Rule: Composition of an IMU
ToDo @Gregory: decide if rule
need to be updated if an IMU with IFM/IFE + IO is possible
An IMU is composed of the following two device types:
-
One main device (circuit breaker or switch ) and an internal ULP communication module
-
One or several external ULP modules
|
A |
PowerPacT H-, J-, L-, P-, or R-frame, or MasterPacT NT/NW circuit breaker |
|
B |
MasterPacT MTZ circuit breaker with ULP port module |
|
C |
MasterPacT MTZ drawout circuit breaker with ULP port module and EIFE interface |
General Rule: Order of ULP Modules in an IMU
Connect the ULP modules in a single IMU in any order. Base the connection on the ULP cable recommendations and the desired layout
for the ULP modules in the electrical equipment.
|
A |
A PowerPacT H-, J-, L-, P-, or R-frame, MasterPacT NT/NW, or MasterPacT MTZ circuit breaker |
General Rule: ULP Line Termination
The ULP modules placed at the end of the ULP line must have a ULP line termination (part number TRV00880) on the unused ULP RJ45 connector.
Place the ULP modules which have an internal ULP line termination at the end of the ULP line, that is:
-
BSCM module or MicroLogic 5 or 6 trip unit for PowerPacT H-, J-, and L-frame circuit breakers.
-
BCM ULP module for PowerPacT P- and R-frame or MasterPacT NT/NW circuit breakers.
-
ULP port module for MasterPacT MTZ circuit breakers.
General Rule: Cables to Interconnect IMUs on Communication Networks
Do not connect the IMUs to one another with ULP cords.
-
Use only the Ethernet cable to interconnect IMUs connected to an Ethernet network.
A
A PowerPacT H-, J-, L-, P-, or R-frame, MasterPacT NT/NW or MasterPacT MTZ circuit breaker
-
Use only the Modbus cable or stacking accessory to interconnect IMUs connected to a Modbus network.
A
PowerPacT H-, J-, L-, P-, or R-frame or MasterPacT NT/NW circuit breaker
General Rule: Power Supply Through the ULP Cord
Only one device can be powered through the ULP cord. This device must be at the end of the ULP line. It can be done only for the following devices:
-
FDM121 display.
-
BSCM module and MicroLogic trip unit for PowerPacT H-, J-, and L-frame circuit breakers.
-
BCM ULP module for MasterPacT NT/NW and PowerPacT P- and R-frame circuit breakers.
|
A |
IFE server |
|
B |
IFM interfaces stacked on IFE server |
|
C |
FDM121 display |
|
D |
IO module |
|
E |
MicroLogic trip unit in PowerPacT H-, J-, and L-frame circuit breaker |
Length of ULP Cords
The rules for ULP cord length are as follows:
-
The maximum length of the ULP cord between two ULP modules in an IMU is 5 m (16.4 ft) if one of the ULP modules does not have an external power supply.
-
The maximum length of the ULP cord between two ULP modules in an IMU is 10 m (32.8 ft) if both ULP modules have an external power supply.
-
The maximum length of all the ULP cords on a single IMU is 20 m (65.6 ft).
-
The bending radius of the ULP cords must be 50 mm (1.97 in) minimum.
Summary of Connection Rules
|
Characteristic |
Value |
|---|---|
|
Connection |
Daisy-chaining of ULP cords and ULP line termination at the end of the ULP line. |
|
Maximum length |
|
|
Voltage range supported |
24 Vdc -10%/+10% (21.6–26.4 Vdc) |
|
300 mA |