New Site Registration

If you are in Energy Access Expert web application home page and you want to add new site, follow the steps in the table:

Step Action

1

Click icon in the home page.


Result: The New Site Registration window is displayed.

2

Select the site type as Villaya Flex and enter the following details in the Site Details tab:

  • EMA SiteID (SiteID captured during the creation process using the EMB tool).

  • Site name and site description.

  • Commissioned date (this date represents the creation date of the site).

3

Enter the details to be updated in the Site Address Details tab.

NOTE: Site address is used to locate the site on the map and to have relevant weather data.

4

Enter the details to be updated in the Site Configuration tab.

5

Select Irradiance Info tab and enter the irradiance data for every month.

NOTE: Irradiance data will differ from month to month and area to area.

6

Click Submit.

Result: The new site is added.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.