Demand Management

Overview

Demand Management: Provides the data on energy consumption and instantaneous readings from the meters (Load, Feeder, or Inverter).

Instantaneous Readings: Provides the latest data received from the smart meter.

Follow the below steps to get energy consumption details and instantaneous reading data:

  1. Open the home page and navigate to PERFORMANCE DASHBOARD > DEMAND MANAGEMENT.

  2. Enter the details to be updated in the DEMAND MANAGEMENT window and click Submit.

Meter Parameter

Parameter

Description

Tariff (KWh)

Provides statistics of energy slabs and slab rates.

TOD

Provides TOD slabs and slab rates for managing power demand during peak load.

Instantaneous Power Limit/Status (W)

Provides the instantaneous power limit and status value from the smart meter.

Energy Limit/ Status (kWh)

Provides the energy consumption limit and status.

Credit Available

Displays the credit available after consumption.

Bar Chart

Energy dashboard shows energy vs. time interval (day, month, year, lifetime, or custom dates) as a bar chart.

Line Chart

Energy data shows energy vs. energy consumption (day, month, year, lifetime, or custom dates) as a line chart.

Trends

Trends provides the data related to instantaneous readings (voltage, current, power, power factor, or frequency).

Report

Click on the top right corner of the window to download the report.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.