Transaction Log

Overview

This feature is used to monitor the transaction history of the devices.

Open the home page and navigate to CONFIGURATION > TRANSACTION LOG.

2-way Transaction

Get Data

Get data logs gives you the present values from the devices, and the user can verify the acknowledgment status. Acknowledgement statuses are successful, in progress, or failed.

Set Data

Set data logs against the customer or device gives you the recently updated new parameter, and the user can verify the acknowledgment status. Acknowledgement statuses are successful, in progress, or failed.

NOTE: Transaction details can be exported in the format of excel , csv file , and pdf files .
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.