Specifications

PC Requirements

Component

Minimum Requirements

Processor

Intel® Core 2 Duo CPU at 3.00 GHz

RAM

4 GB

System type

64 bit or 32 bit

Software Requirements

The following operating systems and web browsers are compatible with the Energy Access Expert for Villaya Flex Application.

  • Microsoft Windows® 7 operating system
  • Microsoft Windows® 8.1 operating system(1)
  • Microsoft Windows® 10 operating system
  • Google Chrome web browser (version 54 or above)
  • Microsoft Edge web browser (version 110 or above).

(1) Local connection with UTA is not supported on Windows 8.1.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.