Reset

Overview

This feature is used to reset device configuration or clear the device data.

Step

Action

1

Open the home page and navigate to CONFIGURATION > RESET.

2

Enter the following details and click RESET:

  • Meter type (load/feeder/inverter)

  • Device mode (energy mode/day mode/all mode)

  • Select the customer and required parameters

    .

3

Click OK.

Result: The device data is reset.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.