Device Control
Overview
This feature is used to get and set the device parameters.
Get Data: Allows you to fetch the latest data of any selected device.
Set Data: Allows you to enter the required parameters and configure the device.
Get and Set Device Parameters
Use Choose File to upload the device configuration parameters.
|
Parameters |
Function |
|---|---|
|
Change Mode |
Allows you to change the modes from day mode to energy mode and vice versa. |
|
Load Credit |
Allows you to recharge the meter (0-9999999). |
|
Credit Days |
Allows you to recharge the meter in days (0-9999). |
|
Set Energy Limit/Day |
Allows you to set the energy limit for a day. |
|
Set Power Limit |
Allows you to set the input power limit for the meter. |
|
Set kWh Slab 1 |
Allows the user to set the first energy slab for Energy Mode. The deduction shall happen from 0 kWh to set Slab 1 kWh at particular set rate. |
|
Set kWh Slab 2 |
Allows the user to set the second energy slab for Energy Mode. The deduction shall happen from set Slab 1 kWh to set Slab 2 kWh at particular set rate. |
|
Set Rate1/kWh Slab 1 |
Allows the user to set the rate at which the credit is deducted for each kWh of energy consumption in Slab 1 (0 kWh to Slab1 kWh). |
|
Set Rate2/kWh Slab 2 |
Allows the user to set the rate at which the credit is deducted for each kWh of energy consumption in Slab 2 (Slab 1 kWh to Slab 2 kWh). |
|
Set Rate3/kWh for above Slab2 |
Allows the user to set the rate at which the credit is deducted for each kWh of energy consumption above Slab 2. |
|
Set GSM Password |
Allow the user to set the Password for SMS commands used for configuring and controlling the dispenser. |
|
SET Key Pad Password |
Applicable only for SEM1500 dispenser model. |
|
TOD* Enabled |
Parameter to enable the TOD feature. NOTE: When TOD is enabled,
the tariffs and Power Limits are applicable during the set time zone
|
|
Set TOD Slab1 |
Parameter to set the 1st TOD time zone (Ex. 08:00 to 09:00) |
|
Set TOD Slab2 |
Parameter to set the 2nd TOD time zone (Ex. 10:00 to 12:00) |
|
Set TOD Slab3 |
Parameter to set the 3rd TOD time zone (Ex. 17:00 to 18:00) |
|
Set Rate1 kWh Slab1 TOD |
Parameter to set the tariff for 1st TOD Time Zone |
|
Set Rate2 kWh Slab2 TOD |
Parameter to set the tariff for 2nd TOD Time Zone |
|
Set Rate3 kWh Slab3 TOD |
Parameter to set the tariff for 3rd TOD Time Zone |
|
SET POWER LIMIT SLAB1 TOD |
Parameter to set the Power Limit for 1st TOD Time Zone |
|
SET POWER LIMIT SLAB2 TOD |
Parameter to set the Power Limit for 2nd TOD Time Zone |
|
Set Power Limit Slab3 TOD |
Parameter to set the Power Limit for 3rd TOD Time Zone |
|
Load Connect or Disconnect (Relay ON/OFF) |
Allows the meter to connect or disconnect the load. |
|
Set Low Balance Alert |
Allows you to set the low balance alert. |
|
GPRS Posting Interval |
Allows the meter to post the data to the cloud for the specified interval values. |
|
Change Entrepreneur Number |
Allows you to change the entrepreneur number. |
|
Change User Number |
Allows you to change the user number. |
|
Auto Clear Credit |
Allows you to clear the credit. |
|
Day to Clear Credit |
Allows the user to clear the credit on particular day of the month. |
|
Overdraft Enable/Disable |
Allows the user to enable or disable the overdraft feature. Overdraft allows the load to run after the credit is expired for a set credit limit or credit day limit. Beyond this limit load is disconnected and the overdraft credit day is deducted from the next recharge. |
|
Overdraft Limit Energy Mode |
Allows the user to set the credit limit for overdraft in Energy Mode. |
|
Overdraft Limit Day Mode |
Allows the user to set the credit day limit for overdraft in Day Mode. |
*Time of Day (TOD) feature is used to manage tariff and power demand during peak load. During peak load duration, a particular tariff and power limit can be set. During a non-peak demand a different tariff and power limit can be set.