Solar Capacity Utilization

This feature displays the total solar utilization of the site.

The capacity utilization factor is the ratio of the actual annual output (in kWh) from a solar plant to the maximum potential output (in kWh) generated under ideal conditions for a year.

The Solar Capacity Utilization is calculated using the following formula:

(PV Consumption / PV Generated) * 100


Generated: Direct PV energy from EMA (KWH)

Could have been generated = Irradiance * PV installed * no. of days

Irradiance: Captured under site configuration

PV installed: Captured under site configuration

No. of days: Number of days since installation (life time value)

NOTE: Number of days varies based on the granular selection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.