Events

Various notification types are displayed on the events tab. Alarms, alerts, or warnings automatically triggers depending on specific devices whenever a meter anomaly or error occurs. The alarms, alerts, or warnings appear under the EVENTS tab.

Active: The alarms, alerts, or warnings that are in active state appears under the Active section.

Historical: The alarms, alerts, or warnings that are resolved and closed appear under the Historical section.

NOTE: Once the active alarms, alerts, or warnings are resolved, the system automatically updates the alarms, alerts, or warnings under Historical.

Resolve: If the Issue is resolved for the alarms, alerts, or warnings that are in the active state, then the user manually enters the remarks and resolves the Issue.

Alarms

Alerts

Warnings

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.