Impact Metrics

Overview

Impact Metrics shows the overall beneficiaries impacted from the site as follows:

  • People Benefited: Displays the total people benefitted from all sites for the selected site type.

    NOTE: For each added customer, four dependent people benefit.

  • Connections: Displays the available connections under the site. There are three types of connections as follows:

    • Residential

    • Community

    • Commercial

  • Entrepreneurs Created: Displays the total entrepreneurs from all sites or selected site. Entrepreneurs are distributors with the privilege to control their customers. Entrepreneur data is defined by the user during the customer creation process. There are two types of entrepreneurs in the system:

    • Men

    • Women

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.