Economic Sustainability

Overview

Economic Sustainability provides the data for accumulated earning and accumulated recharge from the meters at different intervals.

  • Accumulated Recharge:

    Shows the recharges accumulated for the selected meter in the selected interval.
  • Accumulated Earning:

    Shows the credit utilized for the selected meter in the selected interval.

Follow the below steps to get accumulated earning and accumulated recharge data:

  1. Open the home page and navigate to PERFORMANCE DASHBOARD > ECONOMIC SUSTAINABILITY.
  2. Enter the details to be updated in the Economic Sustainability window and click Submit.

Bar Chart

Energy data shows accumulated recharge and accumulated earning vs. time interval as a bar chart.

Line Chart

Energy data shows accumulated recharge and accumulated earning vs. time interval as a line chart.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.