DUG_FLS_LK-01

About the device

The LK FUGA® Wiser wireless battery 4 button switch (hereinafter referred to as Wireless Switch / Freelocate Switch / FUGA Battery Push Button) is a battery-powered wireless switch that is used to control a group of Zigbee devices (such as light and shutter) within the same Zigbee network. The device can be configured through the Wiser app.

Features of the Wireless Switch:

  • Control a group (such as lighting and shutter control).

  • Trigger/activate a moment (such as Movie Night, Good Night Moment).

  • Low battery notification.

NOTE: Construction materials may cause interference which affect Gateway-to-device and device-to-device distances. In the open air, there is no interference, so the distance can be much longer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?