DUG_FLS_LK-01

Moments

A Moment allows you to group multiple actions that are usually performed together. Using the Wiser app, you can create moments based on your needs (such as movie night) and configure them to the Wireless Switch push buttons.
TIP: A moment can be assigned to any of the four keys individually.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?