DUG_FLS_LK-01

Resetting the device

You can reset the Wireless Switch to factory default manually.
To reset the Wireless Switch:
  1. Short press the top-right push button 3 times (< 0.5 s) and then press and hold the push button (>10 s).
  2. After 10 s, LED starts blinking red, then release the push button.
    The wireless switch restarts and blinks green for a few seconds.
    NOTE:
    • After reset, the LED turns off to save the battery.

    • All configuration data, user data, and network data are deleted.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?