DUG_FLS_LK-01

Pairing device manually

Follow the steps to pair the device manually:
NOTE: Remember to insert the battery to turn on the device.
  1. Remove the rockers using the screwdriver to view the LED.
  2. On Wiser app Home page, tap +.
  3. Tap , select Wiser Hub and tap Done.
  4. Select any one of the options to add device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is recommended to add the device with Install Code for security.
  5. To pair the device with an install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code - you can scan the device for the install code.
    • Enter Install Code Manually - you can manually enter the install code from the device.
    After scanning or entering the install code, proceed to Step 7.

  6. To pair the device without install code, tap Add Device without Install Code.
  7. Short press the push-button on top corner 3 times.
    The LED blinks amber.
  8. In the app, select Confirm that the LED is blinking (C) and tap Start Configuration.

  9. After a few seconds, a solid green LED indicates that the device has been successfully paired to the Gateway/Hub.

  10. Once the device is added in the app, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?