DUG_FLS_LK-01

Rotary Dimmer

  1. If you do not need the lower rocker of the Wiser Wireless switch, you can replace it with a blind plate.
  2. Remove the top rocker and short press the left push button 5 times in quick succession on the Wiser Wireless switch.
    The status LED blinks green.
  3. Remove the knob and short press the push button 5 times in quick succession.
    The status LED blinks green.

    The light connected to the Rotary Dimmer blinks for a few times. The status LED stops blinking green on the Wiser Wireless switch and the Rotary Dimmer. The Rotary Dimmer can now be controlled by the Wiser Wireless switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?