DUG_FLS_LK-01

Troubleshooting

Symptom

Possible cause

Solution

LED blinks red.

The Wireless switch battery is low or drained.

Replace the Wireless switch battery.
NOTE: A notification pop–up will appear on the app.

The Wireless switch displays offline in the app.

The Wireless switch battery is low or drained.

Replace the Wireless switch battery.

The Wireless switch is disconnected from the network.

Press any push button on the Wireless switch.

NOTE: The first press does not trigger Wireless switch operation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?