Troubleshooting in Quick Home Connect
|
Symptom |
Possible cause |
Solution |
|---|---|---|
|
LED displays amber on the device. |
Pairing not completed and returned to factory default. |
Pair the Wiser Wireless switch and the device again. Refer to |
|
Wiser Wireless switch not able to control the device reliably. |
The Wiser Wireless switch and the device are too far away from each other. |
Place the Wiser Wireless switch in a position closer to the device. |
|
The Wiser Wireless switch lost pairing. |
Pair the device again. Refer to |
|
|
The Wiser Wireless switch battery is discharged. |
|
Scenario |
Procedure |
|---|---|
|
Control multiple devices with one Wiser Wireless switch. |
To control multiple devices with a single Wiser Wireless switch, start by pairing it with one device. Then, use the same Wireless switch to pair with additional devices. NOTE: You can pair up to 7 devices to a single Wiser Wireless
switch.
|
|
2-gang FLS with devices (relay switch, dimmer, shutter control, or socket outlet). |
Pair either left or right Wireless switch with any of the devices (relay switch, dimmer, shutter control, or socket outlet). You can also pair another rocker of the Wireless switch with another device. |