DUG_FLS_LK-01

Unbinding a moment

Unbinding the moment allows you to remove the moment from the assigned keys without deleting the moment.
  1. In control panel, tap and hold Top right key.
  2. Select the moment and than tap Unbind.
  3. Short press the top right push button 3 times on the Wireless Switch to activate the device and tap Sure on the app notification.

    The moment is now removed from the top right key.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?