DUG_FLS_LK-01

Socket Outlet

  1. If you do not need the lower rocker of the Wiser Wireless switch, you can replace it with a blind plate.
  2. Remove the top rocker and short press the left push button 5 times in quick succession on the Wiser Wireless switch.
    The status LED blinks green.
  3. Short press the push-button of the Socket Outlet 3 times in quick succession
    The status LED blinks green.

    Upon successful pairing, the green LED on the Wiser Wireless switch and the Socket Outlet will stop blinking.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?