DUG_FLS_LK-01

Adding a shutter group

To add a shutter group to the top and bottom right key:
  1. On the Home page, tap All devices > Connected Wireless Switch.
  2. On the control panel page, tap Top right key > Shutter Group > +.
  3. Tap Edit name , enter the group name (A) and tap Save.
    TIP: You can choose the cover image that represents your group by tapping .

  4. Tap Add Task to select any device from the list and tap Next.
    NOTE: You can add one or more actions using .

  5. Once all the actions are set, tap Save.
  6. On the Shutter Group page, select the shutter group (B) you want to assign to the push button.
  7. Short press the top right push button 3 times on the Wireless Switch to activate the device and tap Sure on the app.

    The shutter group is now added to the top and bottom right key (D).

    NOTE: If you add a lighting/moment group to the top/bottom right key, then the app removes the shutter group from the top/bottom right key.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?