SUG_Wiser_Russia_WSE-01

Creating a Moment

This topic explains how to create a Moment.
  1. (See A) In the Home page, tap the icon.

  2. (See B, C) In the Moment page, tap the Moment tab (B) and then tap the + icon (C).

  3. (See D, E) Set a name for the Moment (for example, Welcome) (D) and optionally a background image (E).

  4. (See F, G) Tap Add Task and Run the device to select the device from the All devices list. After you select the required functions in Select Function page, follow the steps in the app.

  5. Tap Save to complete the process to create a Moment.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.