SUG_Wiser_Russia_WSE-01

Configuring voice control — Yandex

Considering Smart Life as an example to introduce how to control smart devices through Yandex Alice, perform the following steps:
  1. Complete product networking configuration in Smart Life App.
  2. Download Yandex App.
  3. Open Yandex and find the Smart Life skill.
  4. Click Smart Life to enter the login page. Enter the account password of the Smart Life App, and click Authorize.
  5. After completing the authorization, set a name for the device and set up a room.
  6. After the setting is completed, you can start voice control equipment, for example: Alice, set your night light to minimum., Alice, turn up the brightness, Alice, switch on a light
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.