SUG_Wiser_Russia_WSE-01

Light switches

Connected Relay Switch 10 A

Controls the lights in a room, or automatically switch lights On or Off in response to a specified condition or event.

Instruction Sheet (PDF)

Device User Guide

Connected Motion Sensor with Switch 10 A

Controls the lights in a room, or automatically switch lights On or Off in response to detected motion, a specified condition or other event.

Instruction Sheet (PDF)

Device User Guide

Wiser Micro Module Light Switch

Converts compatible mechanical push-button switches into smart switches. Connect up to 10 compatible mechanical push buttons.

NOTE: Mechanical push buttons must be certified for use in 220–240 V AC applications.

Instruction Sheet (PDF)


Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.