SUG_Wiser_Russia_WSE-01

Overview of the Wiser™ system

The Wiser system provides an easy, convenient and flexible solution for controlling home devices.

The Wiser gateway (see A) is the center of the system, processing control requests and status reports for connected Wiser devices.

With a personal account and the Wiser by SE app on a mobile phone (see B), users can control the Wiser devices (see C) in their home from any location where the internet is available for both mobile phone and the Wiser gateway.

Wiser devices

The following range of devices are available to provide convenient control of:

  • lighting and dimming

  • motorised shutters and blinds

  • power outlet switching and metering

  • Heating

Sensors are also available to record and report the following:

  • room occupancy

  • ambient light level

  • window/door open or close

  • temperature and humidity

  • water leakage

Device Groups

Operate identical Wiser devices together, either from the local control on one of the devices or by using the .

Use the Group feature in the to combine multiple identical devices and operate them as one. For example, create a group of three Wiser light switches for multi-way operation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.