SUG_Wiser_Russia_WSE-01

Device button/key and LED locations

Find the location of buttons, keys and LED indicators on various devices.

Wiser Micro Module Light Switch/Shades Control

WARNING
Danger due to electric shock
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

(See A) Setup/Reset button

(See B) Status LED

Wiser Micro Module Dimmer

WARNING
Danger due to electric shock
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

(See A) Setup/Reset button

(See B) Status LED

Wiser Window/Door Sensor

(See A) Function key

(See B) Status LED (visible on front of master part when flashing or lit)

Wiser Motion Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser Water Leakage Sensor

(See A) Function key

(See B) Status LED (visible on top of sensor when flashing or lit)

Wiser Temperature/Humidity Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser SmartPlug 16 A

(See A) Operation button

(See B) Status LED

Wiser IP Camera Indoor

(See A) Micro SD Card slot

(See B) Status LED

(See C) Reset Button

Connected Single Socket Outlet 16A

(See A) Reset button

(See B) Status LED

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.