SUG_Wiser_Russia_WSE-01

Devices with motion sensors

Symptom

Possible cause

Solution

Load does not switch on automatically.

NOTE: This does not apply to the battery-powered Wiser Motion Sensor.

Detection brightness for the sensor is low.

Increase the detection sensitivity in device settings.

Load does not switch off automatically when an Automation is triggered.

The Automation may include a delay Action that is set too long.

Reduce the Action delay time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.