SUG_Wiser_Russia_WSE-01

Sensors

Symptom

Possible cause

Solution

The sensor has stopped reporting status, but is otherwise operating normally.

The device may be undergoing an over-the-air (OTA) firmware update.

Wait for the firmware update to complete and then check that the device is reporting status.

NOTE: The firmware update runs in the background.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.