SUG_Wiser_Russia_WSE-01

System requirements for the app

To use the app, your mobile phone must support particular operating systems and versions.

Supported operating systems:

  • Android™ OS version 7 and above
  • Apple® iOS 11 and above
NOTE: When a new version of an operating system is released, it may take some time before the Wiser system is fully compatible with that version.
IMPORTANT:
  • Using Schneider Electric applications with an Android phone that has bypassed restrictions, or a jailbroken iPhone, voids all warranties associated with the application.

  • The compatibility of the interfaces with mobile phones depends on the software version installed on your mobile phone, and may change with a software upgrade. Due to the large number of mobile phones available in the market, the compatibility and functionality of your mobile phone with the app cannot be guaranteed.

NOTE: The app only supports mobile phones, and portrait orientation. Tablet devices such as iPads are not supported.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.