SUG_Wiser_Russia_WSE-01

Checking for any device requiring a firmware upgrade

  1. (See A) On the Home page, tap the Menu icon.
  2. (See B) In the menu slide-out, tap Firmware Upgrade.
  3. (See C) Tap a device in the Devices to be updated list and follow the instructions in the app.
  4. (See D) Tap the button beside Automatically updated to enable automatic updates.
    After this, a notification is received that the firmware is updated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.