SUG_Wiser_Russia_WSE-01

Adding a device

Add a device to a Home by using the app.
NOTE:
  • A gateway must be commissioned and operating before adding a Wiser device.

  • Add mains-powered devices before battery-powered Wiser devices. (See Support for battery-powered devices.)

  • Devices that connect to the network router such as, IP camera, do not require the gateway to be commissioned before add the device.

  1. Log in to the app.
  2. (See A) Select the Home to which the device will be added.
  3. Do one of the following:
    • (See B) In the Home page, tap the + icon (or Add Device if displayed).
    • (See C) From the Wiser Gateway page, tap Add.

  4. (See D) On the Add Device page (D), tap the device you want to add and follow the instructions in the app.
    NOTE: The actual list of devices displayed varies based on different countries.

  5. Do one of the following:
    • (See E) If the device has a visible install code, tap Add Device with Install Code. Scan the install code printed on the device, or enter the code manually, and follow the instructions in the app.
    • (See F) If the device does not have the visible install code then tap Add Device Without Install Code and follow the instructions in the app.

The device is displayed on the Home page as follows:

  • Under a Room tab if the Add Device action was started from that Room

  • Under the All Devices tab if the Add Device action was started from that Wiser Gateway page

Tap the device to access device controls, functions and settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.